Other Parts Discussed in Thread: CC1310
Tool/software: TI-RTOS
We are currently developing a solution which is based on CC1352P. Depending on the usecase our solution will communicate by using 802.15.4 (possible zigbee) – 2,4 Ghz, or 868/915 Mhz using “propmode” or 802.15.4 if available for sub-ghz.
Our solution is targeting the whole world. In order the comply with regulations we are looking at how the CC1352P fits the requirements by FCC, ETSI EN 300 440 and ETSI EN 300 220.
https://www.etsi.org/deliver/etsi_en/300400_300499/300440/02.01.01_30/en_300440v020101v.pdf
https://www.etsi.org/deliver/etsi_en/300200_300299/30022002/03.01.01_30/en_30022002v030101v.pdf
(Paragraph 15.245, 15.247 and 15.249)
Does CC1352P have support for OQPSK DSSS on both sub Ghz and 2,4Ghz?
Which mechanisms does CC1352P and RTOS have built in to transmit with in the +1dBm to +20dBm (or as high as possible)range and still comply with FCC and ETSI using either “digital modulation”, “frequency hopping” or “duty cycling” (or other techniques/mechanisms described by the authorities/standards)?
These questions are relevant for both the 868 Mhz, 915 Mhz and 2,4Ghz bands
Does CC1352P have 802.15.4 support for sub-Ghz frequencies or is “prop-mode” our only option?