This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: CC1200 and 6Lowpan

Part Number: CC1200


Hi,

Hi, 

We are looking for the 6LowPAN Hardware solution with the proven 6LowPAN software stack.

Could you please suggest MCU for the CC1200 Transceiver having

 1. Proven 6LowPAN software stack with the suggested MCU and CC1200

2. 512KB flash, 32KB RAM

3.  Other common peripheral like UART, SPI, I2C

Also you can suggest any other possible solution with similar specs 

Thanks

  • You need a stack in addition to 6LoWPAN which will limit which MCU you can use. We have support for Thread or contiki for some MCU products.

    For Thread, see openthread.io/.../cc2538 for what is supported. CC1352 would also be an option if you want to replace the CC1200 with a wireless MCU but that has a bit less flash than the requirement. What sets the 512 kB limit?

    Contiki (http://contiki-ng.org/ ) is supported on some devices but the MCUs supported generally have not large enough flash.