This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 15.4 Stack: CONFIG_FH_NETNAME question.

Part Number: CC1310

I am wondering what the CONFIG_FH_NETNAME actually does. Is it like an extension to PAN ID?

In normal no-FH modes, there is a requirement that each PAN Co-ordinator has a unique PAN ID among those in vicinity to each other, according to the 15.4 spec. An active scan could determine other nearby PAN Co-ordinators with their respective PAN IDs and then select a unique PAN ID for itself. (The collector example does not seem to add this feature...?).

Anyway, when a sensor joins the collector, the sensor will receive and store the PAN ID of the collector (so the sensor does not need to know this PAN ID in advance). So will the same apply to the CONFIG_FH_NETNAME name? Or must this net name be written in stone at both the collector and sensors in advance?

Is the netname encrypted when transmitted over air? Or can everybody with a packet sniffer detect the name? 

What is the purpose of the netname? And why is it only included in FH modes?

Thanks.

  • Hi,

    The netname is defined by the Wi-SUN spec and they describe it as "The NETNAME-IE is used to match nodes with specifically named FANs. Note that multiple PANs may advertise the same Network Name."
    The net name is embedded in the frequency hoping messages sent by the collector that the joining device uses to get synchronized and be able to join the network. after the device has synchronized and started the joining procedure it will receive the pan ID.
    All sensors need to know the netname before hand because this net name is used as a filter for the synchronization process. similarly you could hard code a PAN ID in the sensor side and it will only join a network with the same pan ID.
    Yes, the net name and all other FH packets are encrypted over the air if you are using security.


    Also, regarding each pan coordinator having a unique panID, the collector example does do an scan at startup to see if there are other pans in the channel and it picks a unique pan ID based on the results of the scan.
  • Thanks for the clarification. I have a specific use case followup question:

    First let's assume that the sensor has associated with the collector since they share the same net name = "NAME_A". Then later the collector decides to change the net name to "NAME_B".

    1. Must the collector restart, or can it still be in normal operation as before the name change?

    2. Will the sensor still be able to communicate with the collector? Will it eventually become orphan?

    3. If I introduce a second sensor, but now with net name = "NAME_B", this will associate with the collector of course. Afterwards I change the sensor net name to "NAME_C". Will this still be able to communicate with the collector?

    The reason I ask is because I would like to use one net name when a sensor associates (for the first time) with a collector. Let's call this net name "JOIN-NAME". When the sensor joins the network, the collector sends the actual net name to be used during normal operation which is a specific net name for the specific network. Then both the collector and sensor change their net name to the specific net name. However, it is important that all the other sensors which already are connected to the network don't loose contact with the collector while the collector temporarily changes net name to "JOIN-NAME". The reason behind this idea is if one sensor looses contact with a collector and becomes orphan, it shall try to associate with another collector belonging to the same customer. If there is another customer nearby I don't want the senor to associate with the other customer's collector. 

    Thanks.

  • I dont think you would have this problem of your devices joining another customer nearby unless both networks are the exact net name and if they are not using security or using the same key for encryption.

    I would recommend you implement an application layer authentication mechanism instead of using the netnames to implement this.
    But if you want to use the netname to do something like this I believe the netname is only used to filter Async messages and you can modify the function "wsAsyncIndCb" accordingly to allow multiple netnames.
  • Thanks. I was also under the impression that only Async messages used the NET NAME (and the Async messages are just used when a sensor wants to join a network or becomes orphan - to my understanding).

    The "issue" arises from ease of manufacturing and sales. We would like to install the same firmware for all devices (sensors and collectors - of course different for the two(!)). The devices shall not require any loading of customer specific parameters before being shipped out - this would otherwise be a huge hassle. The collector will also have a wifi chip (cc3220xx), and the gateway claiming to specific customer has been solved.

    So all of our devices will have the same security key initially and the same net name "out of the box / factory reset". We can also change the security key to be customer specific in the same manner described in the previous post - if this is needed... This may be a better idea than having specific net names - since the net names will solely act as a filter for the async messages. Otherwise we must ensure that all collectors (even the neighbour) have unique PAN ID's. But changing the security keys temporarily when in "claim" mode, would cause all the other normally operating sensors to loose contact with the collector. So the very best solution, perhaps, would be if the collector could have a set of encryption keys consisting of 2 keys. 1 being unique for the network and the other being the common "out of the box" key. The collector would then have to be able to support both key sets simultaneously. Does the stack support this?

    When the customer first takes out the the sensor from the shipment-box, the customer must "claim" the sensor to belong to his/her set of gateway(s). It's in this step the specific "credentials" are transferred from the gateway to the sensor - and hence the GW must temporarily be in "default" mode in order to communicate with the sensor.

    So this is the actual problem definition, and we are trying to solve this issue - provided that a neighbour also has our company's sensors/GW product.

    Another sort of off topic question: It is a requirement that nearby collectors have unique PAN ID's. But can collectors have the same PAN ID, provided that they use security and with different encryption keys? I understand that they will not associate with one another, but will there be more over the air "overhead" due to ACK frames etc - which otherwise would not be present if unique PAN ID's were used?
  • Another observation: When security is enabled, only some types of frames are actually encrypted (verified by wireshark). Hence, "encryption enabled" will not act as a filter for association request frames. However, since there are some more frames involved in the "whole" association procedure - I would assume that the remaining frames are encrypted and ensures that the collector will not add the sensor to its list... I'm not even sure if message integrity code (MIC) is on or off...

    These are the frames which have security:

    STATIC CONST ApiMac_securityPibSecurityLevelEntry_t securityLevelEntry =
        {
          0,
          { MAC_FRAME_TYPE_DATA, MAC_DATA_REQ_FRAME, 0, false }
        };
    /*! Security Level Descriptor */
    typedef struct _apimac_securityleveldescriptor
    {
        /*! Frame Type */
        uint8_t frameType;
        /*! Command Frame ID */
        uint8_t commandFrameIdentifier;
        /*!
         The minimal required/expected security level for incoming MAC frames.
         */
        uint8_t securityMinimum;
        /*!
         Indication of whether originating devices for which the Exempt flag is
         set may override the minimum security level indicated by the Security
         Minimum element. If TRUE, this indicates that for originating devices
         with Exempt status, the incoming security level zero is acceptable.
         */
        bool securityOverrideSecurityMinimum;
    } ApiMac_securityLevelDescriptor_t;

    Where can I find all the possible security constant values for both frameType and commandFrameIdentifier? The example only lists MAC_FRAME_TYPE_DATA and MAC_DATA_REQ_FRAME. I have tried to find the list of possible values here, but have not found any: dev.ti.com/.../struct__apimac__securityleveldescriptor.html

  • Hi,

    You can find all the definitions for the frame types in the file mac_spec.h. 

    /* Command frame identifiers */
    #define MAC_ASSOC_REQ_FRAME             1
    #define MAC_ASSOC_RSP_FRAME             2
    #define MAC_DISASSOC_NOTIF_FRAME        3
    #define MAC_DATA_REQ_FRAME              4
    #define MAC_PAN_CONFLICT_FRAME          5
    #define MAC_ORPHAN_NOTIF_FRAME          6
    #define MAC_BEACON_REQ_FRAME            7
    #define MAC_COORD_REALIGN_FRAME         8
    #define MAC_GTS_REQ_FRAME               9
    #define MAC_ENHANCED_BEACON_REQ_FRAME   10

    Also the stack does support storing multiple keys. So yes you can keep the default key for joining devices and then update the network key in the new sensors by sending the new key over the air.

    Collectors pick a unique PAN ID based on the surrounding networks. A collector will send a beacon request the very first time that it is powered up and it records all PANIDs from the incoming beacons from other networks and it selects a PAN ID that is different from all nearby networks. I believe the "algorithm" for picking a PAND ID is just the highest nearby PAN ID + 1.

    it is possible to have 2 different networks with the same PAN ID which will happen in the scenario that both networks were brought up out of range from each other and then brought within range. This will cause problems mainly if devices in both networks have the same short addresses. Even if both networks have different encryption keys, all devices with the same PANID & same short address will ack packets targeted for their short address.