Other Parts Discussed in Thread: C2000WARE, CC1200
Hi,
I'm using a F28379D with a CC1200EMK. Reading and writing from a single (non extended) register seems to behave in an odd way. For example, when I read/write to IOCFG3, 0x01, 0x06 and 0x03 work, but 0x02 and 0x04 fail. Also, when I try this with other registers, sometimes it fails. I'll post two examples below, one of the IOCFG3 and one of CHAN BW registers.
My process currently is:
Pull CSN low, wait for MISO to go high, delay 0.5 Us, start transmission. Write to the address. Once done, Read from the address.
Some additional information: I'm using the C2000Ware Driverlib for my SPI. 4 MHz clock speed. SPIA_LOW and SPIA_HIGH etc use an external GPIO for the CS_n of the CC1200.
The status returned with both of these tests is 0x60.
Code: (ICOFG3)
while ( final_value != 0x03) // To repeat this with a breaking point
{ SPIA_LOW; SPIA_WAIT; DEVICE_DELAY_US(1); // WRITE TO ADDRESS SPI_writeDataBlockingNonFIFO( current_base, 0x0000); // IOCFG3 DEVICE_DELAY_US(0.5); // Delay SPI_writeDataBlockingNonFIFO(current_base, 0x02<<8); // READ FROM ADDRESS DEVICE_DELAY_US(1); SPI_writeDataBlockingNonFIFO(current_base, 0x80<<8); write_return_value = SPI_readDataNonBlocking(current_base); DEVICE_DELAY_US(0.5); write_return_value_2 = SPI_readDataNonBlocking(current_base); //SEND A DUMMY BYTE SPI_writeDataBlockingNonFIFO(current_base, 0xFF<<8); DEVICE_DELAY_US(0.5); before_final_value = SPI_readDataNonBlocking(current_base); DEVICE_DELAY_US(0.5); final_value = SPI_readDataNonBlocking(current_base); SPIA_HIGH; DEVICE_DELAY_US(10); }
Another example with CHANBW register, this code returns 0xF7
while ( final_value != 0x03) { SPIA_LOW; SPIA_WAIT; DEVICE_DELAY_US(1); // WRITE TO ADDRESS SPI_writeDataBlockingNonFIFO( current_base, (CC120X_CHAN_BW | CC1200_WRITE_BIT) << 8); // IOCFG3 DEVICE_DELAY_US(0.5); // Delay SPI_writeDataBlockingNonFIFO(current_base, 0xA6<<8); // READ FROM ADDRESS DEVICE_DELAY_US(1); SPI_writeDataBlockingNonFIFO(current_base, (CC120X_CHAN_BW | CC1200_READ_BIT) <<8); write_return_value = SPI_readDataNonBlocking(current_base); DEVICE_DELAY_US(0.5); write_return_value_2 = SPI_readDataNonBlocking(current_base); //SEND A DUMMY BYTE SPI_writeDataBlockingNonFIFO(current_base, 0xFF<<8); DEVICE_DELAY_US(0.5); before_final_value = SPI_readDataNonBlocking(current_base); DEVICE_DELAY_US(0.5); final_value = SPI_readDataNonBlocking(current_base); SPIA_HIGH; DEVICE_DELAY_US(10); }