This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1350: sensor node identity for the collector

Part Number: CC1350


Hi,

     I wanted to know if the broadcast packages can be sent to the certain specific sensors which are supposed to be connected to a particular collector? Because I want to connect to 250 nodes and don't want to create extra traffic from the adjacent network of 250 nodes.What i mean to say is that if there is another collector in the range of the sensors which are to be connected to a particular collector a huge amount of traffic will be created.Please correct me if I am wrong and also suggest a solution

Thanks And Regards

Stuti Jain