This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: tidc01002 SimpleLink™ Sub-1 GHz Sensor to Cloud Gateway Reference Design

Expert 4011 points
Part Number: CC1310

Hi,

I was following the design guide and got stuck in the 3.2.1.1.8 Set Up Node.js Cloud Foundry App

Step 6.Push the code to the IBM cloud foundry app: cf push
...

Exit status 0
Staging complete
Uploading droplet, build artifacts cache...
Uploading build artifacts cache...
Uploading droplet...
Uploaded build artifacts cache (6.1M)
Uploaded droplet (32M)
Uploading complete
Stopping instance 3b1f3d8f-135b-4e97-bfdf-8e0ef99b8505
Destroying container
Successfully destroyed container

0 of 1 instances running, 1 starting
0 of 1 instances running, 1 starting
0 of 1 instances running, 1 starting
0 of 1 instances running, 1 starting
0 of 1 instances running, 1 starting
0 of 1 instances running, 1 crashed
FAILED
Error restarting application: Start unsuccessful

TIP: use 'cf logs CC3220SFdemoAtIoTSeminarSep2018 --recent' for more information

The log data is in attachment. Please help to check it out and advise.

Programming started....
Executing the following command:
> "C:\ti\uniflash_8.3.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\DSLite" flash -c "C:\Users\alexk\Centrica\Everyone Israel - HW - HW\HW\ATE\Documentation\Auxiliary boards\FlashPro430 vs XDS110 Adapter\CC1312_TargetConfiguration_500kHz.ccxml" -l "C:\ti\uniflash_8.3.0\My Laptop package\user_files\settings\generated.ufsettings" -e -v -f "C:\Users\alexk\Desktop\CC-1311 programing\EVB\Peripherals test\Example_test_for_Panoramic_power.bin"

For more details and examples, please refer to the UniFlash Quick Start guide.

DSLite version 12.3.0.3041
Configuring Debugger (may take a few minutes on first launch)...
        Initializing Register Database...
        Initializing: IcePick_C
        Executing Startup Scripts: IcePick_C
        Initializing: CS_DAP_0
        Executing Startup Scripts: CS_DAP_0
        Initializing: Cortex_M4_0
        Executing Startup Scripts: Cortex_M4_0
Connecting...
Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
Cortex_M4_0: GEL Output: Board Reset Complete.
Failed: Encountered a problem loading file: C:\Users\alexk\Desktop\CC-1311 programing\EVB\Peripherals test\Example_test_for_Panoramic_power.bin
Could not determine target type of file

C:\ti\uniflash_8.3.0>