This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC1350: CC1350 : USE frequency (447mhz)?

Part Number: CC1350

Tool/software: TI-RTOS

Hi,

I have question about CC1350.

# USE Frequency question......

  In the datasheet for CC1350 the following frequency bands are noted:

  1)  1.1 Features 1
       World's First Dual-Band (Sub-1 GHz and 2.4 GHz)

  2) 1.2 Applications

      315-, 433-, 470-, 500-, 779-, 868-, 915-, 920-MHz and 2.4-GHz ISM and SRD Systems

=> Then, If you look at  2), is this not possible to use 447MHz band?

=> Can you tell me about other products that can use 447MHz(SoC or transceiver)?

-Thank you, sir- END-