Hello,
I am using CC1352R1 contoller. In rfPacketTx_CC1352R1_LAUNCHXL_tirtos_ccs example code i integrated uart code. uart Tx is working but RX is not working, not getting interrupt. This is uart code
UART_Params_init(&uartParams);
uartParams.baudRate = 115200;
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY ;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.readMode= UART_MODE_CALLBACK;
uartParams.writeMode=UART_MODE_CALLBACK;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readTimeout=UART_WAIT_FOREVER;
uartParams.readCallback=uartCallbackFunction;
uartParams.writeCallback=uartwriteCallbackFunction;
uart = UART_open(Board_UART0, &uartParams);
if
(uart == NULL)
{
/* UART_open() failed */
while
(1);
}
UART_control(uart, UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE, NULL);
UART_read(uart, Uart_Rx_Buff,100);