Part Number: CC85XXDK-HEADSET
Dear TI Experts,
My customer is evaluating CC8530 with 2pcs CC85XXDK-HEADSET. They found that the EVM's communication distance is only about 20~30m. They've tried to raise the supply voltage from 2.15V to 3.3V, change SDK to B version from A version, however, the communication distance only got a lillte improvement. They measured the output power from EVM, it is around 10dbm. Could you kindly advise how to improve the communication distance to 50m based on TI's CC85XXDK-HEADSET EVM? Thanks a lot. Once achieve 50m in EVM, they will build their own CC8530+CC2590 board.