This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC1310: collector and sensor communication fail

Part Number: CC1310

Tool/software: TI-RTOS

Dear Sir,

SDK : 1_60_00_21 ( TI_15.4 stack )

Device information : CC1310 launchpad

Example projects : Collector and Sensor

I was try to use CC1310 collector/sensor example code, and i was find out two problem as below.

1. When collector update F/W finish ( use SBL ), and re-stored network information and sensor list to collector.

I was find out sensor can uplink data, but can't receive response form collector, it was only be normal when re-power cycle the sensor.

P.S : Sniffer log as below.

  

Packet No.13 : Sensor send request data to collector

Packet No.23 : Collector send response data to collector

Packet No.37 : Sensor RE-SEND request data to collector because it doesn’t receive response from Collector

Packet No.47 : Collector send response data to collector

 

!!!! Repower cycle the Sensor

 

Packet No.195 : Sensor send request data to collector

Packet No.201 : Collector send response data to collector   (Sensor receive the response data, stop RE-SEND )

 

2.  When sensor was association with collector already, then reset sensor device, 

the collector can’t get any data payload when re-connection.

Is there anyone can help me