This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/SIMPLELINK-CC13X0-SDK: Use Analog comparator in CC1310

Part Number: SIMPLELINK-CC13X0-SDK

Tool/software: TI-RTOS

Hi!

Possible reasons not to use sensor controller to obtain the result from comparator:

1. Absence of any example in SCS for the comparator.

2. Sensor controller can be busy with other tasks.

3. The need to quickly change the threshold of the comparator.

4. If noRTOS comparator driver has ten lines of asm code, why should I install and study heavy and unclear SCS?

I would like to see an example of working with comparator registers and changing the threshold.

Best regards,

Orl.