This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1350: No able to run the code without Debugger

Part Number: CC1350

Tool/software: Code Composer Studio

Hi,

    I have designed a custom board using cc1350 and I am testing with the example application of sensor_1350lp.When the debugger is running the code works even If I stop the debugger it will work.But if a power reset happens and again I power it up by JTAG only the code doesn't work. Whereas if I download standby pin interrupt or any other code which RF like RFWSNNODE.The code works even after a power reset.I am not able to understand what the issue is .It would be really great if somebody could help me with this.

Most of the links which I found are with reference to the BLE example .

Thanks And Regards

Stuti