Hi,
We have developed a low power remote control with a CC110L module. The wireless communication is working like it should, but we have received reports from the field where battery are empty after only 2 weeks. These should normally last 2 years. We are checking the code on our microcontroller, but everything seems in order.
One possible cause that we thought off, is a reset of the CC110L chip. We only initialize the RF chip once at boot (power up). If the RF chip resets, it isn't in low power mode anymore and it will drain the battery. Do you have encountered previous reports of spontaneous resets of the CC110L chip?
We haven't been able to reproduce the issue and also at that moment it is very difficult to read the CC110L configuration.