I have been testing some of our units that use a CC1101 using a CCDebugger that we have had for a while. Everything works well. However, I ordered two more CCDebuggers , and neither of them work to connect to our hardware. The CCDebugger is recognized, but the CC1101 conected to it is not. The LED remains red. Is there some sort of update that I need to do to the firmware in order to get them to work? If it had only been one I might be inclined to blame it on bad debugger HW, but since it's both I'm guessing it's something else.