This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/LAUNCHXL-CC1310: Linux/LAUNCHXL-CC1310 onboard XDS100 debugger

Part Number: LAUNCHXL-CC1310

Tool/software: Linux

Hi,

I just got couple of LAUNCHXL-CC1310 following boards:

Rev: 1.4.1

PG 2.1

FW Rev: 1.0

1733

I didn't manage to make XDS100 onboard debugger working under x64 Ubuntu Linux, regardless of driver install or any procedure described here.

What bothers me is TI known issue note

"

Known Issues

  • XDS100v1 debug probes are not compatible with Ubuntu 16. We are working with FTDI to resolve this.

"

On my system after all drives installed as root I still get: "Cortex_M3_0: Failed Board Reset: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed"

When do " > lsusb " command in terminal I see there is some Texas device on the bus: "Bus 001 Device 038: ID 0451:bef3 Texas Instruments, Inc." So there seems to be at least USB cable connection to the LAUNCHPADXL-CC1310 board.

However there is no virtual com port listed, but my main priority is to make XDS100 onboard debugger working first.

Any Ideas what could be wrong and how to make the XDS100 onboard debugger working under linux, is it actually supported or are there any other known issues?

Thanks,

BR