This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: At which frequency is the CC1310 launchpad better matched, 868 MHz or 915 MHz ?

Part Number: CC1310

Hello,

Can you please tell me at which frequency is the CC1310 launchpad's antenna better matched, 868 MHz or 915 MHz ? According to my measurements, there is a difference. Actually, one year ago, when I first bought the launchpad, I remember reading somewhere that there are different CC1310 launchpads where each one of them is better matched at a specific frequency but I am not sure.

Thank you!

Brinix