This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1350: cc1350

Part Number: CC1350

Tool/software: Code Composer Studio

hi,

i would like to use the cc1350 uart. I started from the nortos uart echo example.

I am able to send bytes on the uart (I checked with the oscilloscope) using the uart_write call, but when I call the uart_read the procedure does not return. 

I am worry that an interrupt occur but I do not see any interrupt procedure, what happen is:

- if the TXD is connected to RXD when I call the uart_read the program will not return (I am using the cc1350 launchpad board in debugging)

- if the TXD is not connected to RXD the uart_read return but clearly with no data.

N.B. I set the pin DIO2 and 3 as uart rx and tx

well:

1) is correct my analysis?

2) can i work with no interrupt (can I have help about it)?

3) any other suggestions?

thank you

maurizio stefani