Tool/software: Code Composer Studio
I used the CC1310F128RGZ (48-Pin package) on a previous design, and everything worked well.
I needed to shrink the design into a smaller package, and switched to the CC1310RHBT (32-Pin device, 5x5mm).
With the new 32-pin design the crystal does not oscillate - all circuitry is the same (inductor, crystal, caps, etc).
Does not seem to be a hardware issue, as the device will run in debug mode using CCS and Spectrum Digital XDS100V3 (crystal is oscillating when running in debug mode).
Tried various hardware resets after power up with no effect.
Crystal still oscillates when exiting debug mode, but will not oscillate from power up in normal mode.
Any thoughts or tests you can recommend to isolate this problem?
I am using the same crystal as was used in the 48-pin design, and have tried several boards.
Seems that if it runs in debug mode, it would run in standalone mode.
Thanks.