Hello,
customer wants to use the RCOSC as input for the RTC. He wants to calibrate it against the 24MHz osciallator. Is there a RCOSC calibration routine in C code which I can use? How often should it be run?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
customer wants to use the RCOSC as input for the RTC. He wants to calibrate it against the 24MHz osciallator. Is there a RCOSC calibration routine in C code which I can use? How often should it be run?
Regards, Holger
Hi Holger,
When waking up from standby, the power driver will calibrate the RCOSC. You only need to call the function yourself if you need to re-calibrate it for some reason (extended period of time out of standby).
The exact duration of this function is hard to say as it would depend on the state of the calibration. The worst case scenario the Power driver expect when waking from standby, including calibration and re-powering the device is ~1ms, this should at least put an upper limit to what to expect for the calibration.
Hello M-W,
just for confirmation. Eg: Customer plans a long standby time may be 1min. Then he wants to calibrate the RCOSC in between all 10s. He just has to wake up the CC1310 and then go in stanby again? The power driver is doing the calibration by its own? I don't have to call this function in my SW?
Regards, Holger