This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: 32K Crystal Lord Capacitance

Part Number: CC1312R
Other Parts Discussed in Thread: TIDA-010024

Hi team,

 I checked the schematic of TIDA-010024, the external capacitance is 15pF at X32K_Q2.  The maximum value in datasheet is 12pF.
 The question is the definition of 32K Crystal Load Capacitance in datasheet (Table 5-4) is for external capacitance or internal capacitance value? 

Regards,
Ogasawara