I have two Launch XL CC1350-4 boards
The first board I have had for a while and initially ran the BLE stack and application on it and this ran fine.
Then I tried some other examples and a project of my own derived from a sample.
Recently I went back to wanting to use this board for BLE and flashed the stack and simple peripheral in that order.
It partially works in that it advertises but when I attempt to connect I get an immediate disconnect.
Fortunately I had another identical Launch XL CC150-4 board that I had never used. I did the same flashing as above to it and it works fine.
As it does not appear that there is any hardware differences (all jumpers same, and no component changes) I am assuming that there is something different in the flash between the two that is causing this issue.
What I guess I am looking for is a complete (all flash memory) flash image that gets the LaunchXL CC1350-4 back to how it came from the factory?
Thanks,
Shawn