Other Parts Discussed in Thread: CC1100
I'm working with a customer who is in the process of preparing for the regulatory testing of a product with the CC1101 (upgraded from the CC1100).
DN009 “Upgrade from CC1100 to CC1101” states “CC1100 can be replaced by CC1101 without changing register settings.” Based on that, I planned on using the same code for both. However, I thought I would check the power table settings in DN012 and DN013 since we give the test house a variety of values to try. The power levels are different for the same register setting. We have been using 0x8A which is 2.6 dBm for the CC1100 and 1.8 dBm for the CC1101 at 915 MHz. At 868 Mhz the CC1100 is 3.0 dBm and the CC1101 is 2.1 dBm. Is keeping the value the same going to make any significant change in the range or power used by the new chip?
Thanks,
Stuart