This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: reading MAC address from a custom program

Part Number: CC1310

In order to generate print labels for my modules (has CC1310), I need to manually use "flash programmer 2" to read the primary IEEE 802.15.4 MAC address. I will write a simple C++ code to perform the MAC (EUI64) address to generate the labels. What tool can I use on Windows 10 to perform the MAC addr read, is it XDC tool? Is there already a sample/example code for it?