This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Correct packet length in the SmartRF studio 2.10.0

Part Number: CC1310


Hello,

There is something that I do not quite understand in the SmartRF studio GUI. When I first start it, I see 30 Bytes of data in the packet. When I click the "code export" button, I see two variables:

- pktLen : 30

- Packet Length: 20

Why are they different? what is the actual number of data bits being transmitted?

And what is the difference between a fixed and a variable length configuration?

Thanks,

Brinix