Hello,
My customers are trying to change the parameter of TOC_CFG.TOC_LIMIT from 00 to 01.
To change the parameter, do they need to set the additional parameter?
Especially, we want to know the default settings of TOC_CFG.TOC_PRE_SYNC_BLOCKLEN and TOC_CFG.TOC_POST_SYNC_BLOCKLEN in case of changing TOC_CFG.TOC_LIMIT to 01.
And is there any bad influence by changing the parameter?
They are using CC1200 as a receiver.
Because the transmitter's reference clock source is a RC oscillator, the variation of frequency is very large.
As a result, in case TOC_CFG.TOC_LIMIT is 00, the receiver (CC1200) cannot receive the many packets.
Best Regards,
Nomo