This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

#CC1310, #TI 15.4

Part Number: Rejoin Error

I've setup a collector/sensor system with the reference projects.

I've notice the sensor does not consistently send the association request to collector.

After the sensor joins our collector, I leave the system running and everything executes on the proper interval.  I then reset the sensor.  Most of the time the sensor will send the PCS and receives the PC from the collector.  Then the sensor will send the association message and rejoin the network.

However, sometimes after receiving the PC the sensor does not initiate the association message.

Our test instrument see's the PCS and the message from the collector indicates the PCS was received and sends it PC message.   On the sensor side we see the PC was received but does not start the association.

This occurs roughly 1 in 20 rejoin test.