Other Parts Discussed in Thread: CC1200,
Hi
I send a data packet from cc1200 evaluation borad and receive that data in ook modulation without manchester codding.
But when i send that data with the same frequency and symbol rate in manchester code and set cc113l in manchester decode enable, I receive no valid packet with cc113l.
Cc113 config is:
Base frequecy:433.99 Mhz
Rx filter BW : 833.33 khz
Xtal frequency:26Mhz
Data rate:12.3 kbaud
In transmiter also configs are:
Symbol rate 12.3 ksps
Bit rate : 6.15kbps
I hope somone help me solve the problem.