This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1312R1: Issue in OAD device firmware upgrade.

Part Number: LAUNCHXL-CC1312R1


I have created network using two CC1312R1 LAUNCHXL with the help of TI 15.4 Stack. I have connected one CC1312 with raspberry pi zero which will act as a gateway. 

I am using TI 15.4 Stack Linux gateway application in raspberry pi and sensor code at the other CC1312 which is working perfectly.

My main concern is to upgrade firmware at the sensor side using Over the Air Download. 

I copied "sensor_oad_cc1312r1lp.bin" image file which is generated by CCS into raspberry pi.

then I run the collector and gateway app on raspberry pi. I am attaching the snaps from collector and sensor below.

  

I located the file using "f" command and then send the update request with "u" command. I got this on terminal.

on completion I receive this

Now the Problem is after successfully receiving OAD Block the sensor board is not rebooting. It is not connecting to the network even after I reset it. It seems the older image has been erased but the new image hasn't been loaded. Hoping to receive positive response.

Thanks and Regards,

Mitul Parmar