Hi, I'm using SimpliciTI with CCSv4 on ez430-rf2500. I tried running the Simple Peer-to-Peer sample following the instructions in SimpliciTI Sample Application User's Guide, but it didn't work. Are the talker (LinkTo) and listener (LinkListen) supposed to have the same or different addresses? I tried setting both addresses to {0x78, 0x56, 0x34, 0x12}, then one with {0x78, 0x56, 0x34, 0x12} and the other with {0x87, 0x56, 0x34, 0x12} and vice versa but it still doesn't work. I push the button on the listener, then I push it on the talker, but then the talker's LEDs just keep blinking.