Tool/software: Code Composer Studio
Good afternoon,
we have a customer board mounting a CC1310 and we debug it by the XDS on the LaunchPad CC1310.
We connect the customer target by the connector P7, and we have removed all the jumper P4 of the LaunchPad.
Our problem is that a lot of customer board have problems after we have debugged them for a while. We are not able to identify the problem, also because when they stop to work, they have different behaviour. For example, the last board killed is recognized from the SmartRF Studio, but when we tried to load it by CCS we have the message below. Please, have you got any suggestion to investigate about the problem?
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Target timed out! (Block 0)
Cortex_M3_0: Status 0x0103: Target flashloader failed to program flash. Low level function returned status 4 (Operation failed).
Cortex_M3_0: Command=4 -- addr=0x00001000 -- length=0x00001000
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
Cortex_M3_0: GEL: File: C:\Projects\IRSAP\project\workspace_ti_ccs\rfIrsapNow20Meh\Now20Meh_Debug_Cli\rfIrsapNow20Meh.out: Load failed.
Have you got any suggestion to try to understand the problem?