Hello,
What registers need to be changed to configure the CC1310 for 5kbps LRM. We are using the sensor/collector example code as a baseline to run some tests.
In RF smart Studio, it provides some preconfigured radio setups for the CC1310. Is there any way we can port these radio setups directly into our custom code builds without having to figure out all of the individual register setting adjustments?
The one we want specifically is 5 kbps, SimpleLink Long Range (20 kchip/s, 2-GFSK, conv. FEC r=1/2 K=7, DSSS SF=2, Tx dev.: 5 kHz, Rx BW: 49 kHz)
Thanks,
Nick