Hello,
I'm trying to connect CC1310 to pc via uart while debugging in IAR.
I use smartRF06 Evaluation board.
From smartRF06 documentation I found that 2 com ports needs to be in device manage.
After I installed the "SmartRF studio 7" I see only one com port.
what should I do to connect the serial monitor in my PC with the device uart output.
I use the driver uart example as device code.
Vitaly