This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC1310: Tx Power value is getting Low

Part Number: CC1310

Tool/software: TI-RTOS

Hi,

    We are transmitting the data in 433MHz. Here we are facing two issues those are

1. We are setting Tx power as 15dBm in the Smart RF studio and doing continuous Tx and then we are measuring in the spectrum analyzer it is showing 9dBm only. what might be an issue?

2. And the next is, Instead of doing continuous Tx from smart RF studio, we have programmed "rfPacketTx" example code with Tx power as same 15dBm(.txPower = 0x913F, .centerFreq = 0x01B1, .loDivider = 0x0A in smartrf_settings.c) then we are measuring in spectrum analyzer it is showing 8dBm only. Is there any other setting do we need to change??

Regards,

Harsha