Tool/software: TI-RTOS
Hello, I use TX an RX examples to do my follow code:
#include <unistd.h> #include <stdint.h> #include <stddef.h> #include <stdlib.h> /* Driver Header files */ #include <ti/drivers/rf/RF.h> // #include <ti/drivers/GPIO.h> #include <ti/drivers/PIN.h> #include <ti/drivers/pin/PINCC26XX.h> #include <ti/drivers/timer/GPTimerCC26XX.h> // #include <ti/drivers/I2C.h> // #include <ti/drivers/SDSPI.h> // #include <ti/drivers/SPI.h> // #include <ti/drivers/UART.h> // #include <ti/drivers/Watchdog.h> /* Driverlib Header files */ #include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h) /* Board Header file */ #include "Board.h" #include "RFQueue.h" #include "smartrf_settings_433MHz/smartrf_settings.h" #define PAYLOAD_LENGTH 30 /* Packet RX Configuration */ #define DATA_ENTRY_HEADER_SIZE 8 /* Constant header size of a Generic Data Entry */ #define MAX_LENGTH 30 /* Max length byte the radio will accept */ #define NUM_DATA_ENTRIES 2 /* NOTE: Only two data entries supported at the moment */ #define NUM_APPENDED_BYTES 2 /* The Data Entries data field will contain: * 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1) * Max 30 payload bytes * 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */ static void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e); static RF_Object rfObject; static RF_Handle rfHandle; static PIN_Handle ledPinHandle; static PIN_State ledPinState; /* Buffer which contains all Data Entries for receiving data. * Pragmas are needed to make sure this buffer is 4 byte aligned (requirement from the RF Core) */ #pragma DATA_ALIGN (rxDataEntryBuffer, 4); static uint8_t rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES, MAX_LENGTH, NUM_APPENDED_BYTES)]; /* Receive dataQueue for RF Core to fill in data */ static dataQueue_t dataQueue; static rfc_dataEntryGeneral_t* currentDataEntry; static uint8_t packetLength; static uint8_t* packetDataPointer; static uint8_t packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1]; /* The length byte is stored in a separate variable */ //static uint8_t packet[PAYLOAD_LENGTH]; static uint16_t seqNumber; PIN_Config pinTable[] = { Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX, Board_PIN_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX, PIN_TERMINATE }; static int accion; //accion=0 (transmision) //accion=1 (recepcion) /* * ======== mainThread ======== */ void *taskLedToggleTimer(void *arg0) { /* Call driver init functions */ RF_Params rfParams; RF_Params_init(&rfParams); ledPinHandle = PIN_open(&ledPinState, pinTable); if (ledPinHandle == NULL) { while(1); } if(RFQueue_defineQueue(&dataQueue, rxDataEntryBuffer, sizeof(rxDataEntryBuffer), NUM_DATA_ENTRIES, MAX_LENGTH + NUM_APPENDED_BYTES)) { /* Failed to allocate space for all data entries */ while(1); } RF_cmdPropTx.pktLen = PAYLOAD_LENGTH; RF_cmdPropTx.pPkt = packet; RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW; /* Modify CMD_PROP_RX command for application needs */ /* Set the Data Entity queue for received data */ RF_cmdPropRx.pQueue = &dataQueue; /* Discard ignored packets from Rx queue */ RF_cmdPropRx.rxConf.bAutoFlushIgnored = 1; /* Discard packets with CRC error from Rx queue */ RF_cmdPropRx.rxConf.bAutoFlushCrcErr = 1; /* Implement packet length filtering to avoid PROP_ERROR_RXBUF */ RF_cmdPropRx.maxPktLen = PAYLOAD_LENGTH; RF_cmdPropRx.pktConf.bRepeatOk = 0; RF_cmdPropRx.pktConf.bRepeatNok = 0; /* Request access to the radio */ rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams); /* Set the frequency */ RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0); accion = 0; seqNumber=0; while (1) { if(accion == 0) { packet[0] = (uint8_t)(seqNumber >> 8); packet[1] = (uint8_t)(seqNumber++); uint8_t i; for (i = 2; i < PAYLOAD_LENGTH; i++) { packet[i] = i - 2; } /* Send packet */ RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0); switch(terminationReason) { case RF_EventLastCmdDone: // A stand-alone radio operation command or the last radio // operation command in a chain finished. break; case RF_EventCmdCancelled: // Command cancelled before it was started; it can be caused // by RF_cancelCmd() or RF_flushCmd(). break; case RF_EventCmdAborted: // Abrupt command termination caused by RF_cancelCmd() or // RF_flushCmd(). break; case RF_EventCmdStopped: // Graceful command termination caused by RF_cancelCmd() or // RF_flushCmd(). break; default: // Uncaught error event while(1); } uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropTx)->status; switch(cmdStatus) { case PROP_DONE_OK: // Packet transmitted successfully PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1)); accion=1; break; case PROP_DONE_STOPPED: // received CMD_STOP while transmitting packet and finished // transmitting packet break; case PROP_DONE_ABORT: // Received CMD_ABORT while transmitting packet break; case PROP_ERROR_PAR: // Observed illegal parameter break; case PROP_ERROR_NO_SETUP: // Command sent without setting up the radio in a supported // mode using CMD_PROP_RADIO_SETUP or CMD_RADIO_SETUP break; case PROP_ERROR_NO_FS: // Command sent without the synthesizer being programmed break; case PROP_ERROR_TXUNF: // TX underflow observed during operation break; default: // Uncaught error event - these could come from the // pool of states defined in rf_mailbox.h while(1); } } else{ RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRx, RF_PriorityNormal, &callback, RF_EventRxEntryDone); switch(terminationReason) { case RF_EventLastCmdDone: // A stand-alone radio operation command or the last radio // operation command in a chain finished. break; case RF_EventCmdCancelled: // Command cancelled before it was started; it can be caused // by RF_cancelCmd() or RF_flushCmd(). break; case RF_EventCmdAborted: // Abrupt command termination caused by RF_cancelCmd() or // RF_flushCmd(). break; case RF_EventCmdStopped: // Graceful command termination caused by RF_cancelCmd() or // RF_flushCmd(). break; default: // Uncaught error event while(1); } uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropRx)->status; switch(cmdStatus) { case PROP_DONE_OK: // Packet received with CRC OK /* Toggle pin to indicate RX */ PIN_setOutputValue(ledPinHandle, Board_PIN_LED2, !PIN_getOutputValue(Board_PIN_LED2)); accion=0; sleep(1); break; case PROP_DONE_RXERR: // Packet received with CRC error break; case PROP_DONE_RXTIMEOUT: // Observed end trigger while in sync search break; case PROP_DONE_BREAK: // Observed end trigger while receiving packet when the command is // configured with endType set to 1 break; case PROP_DONE_ENDED: // Received packet after having observed the end trigger; if the // command is configured with endType set to 0, the end trigger // will not terminate an ongoing reception break; case PROP_DONE_STOPPED: // received CMD_STOP after command started and, if sync found, // packet is received break; case PROP_DONE_ABORT: // Received CMD_ABORT after command started break; case PROP_ERROR_RXBUF: // No RX buffer large enough for the received data available at // the start of a packet break; case PROP_ERROR_RXFULL: // Out of RX buffer space during reception in a partial read break; case PROP_ERROR_PAR: // Observed illegal parameter break; case PROP_ERROR_NO_SETUP: // Command sent without setting up the radio in a supported // mode using CMD_PROP_RADIO_SETUP or CMD_RADIO_SETUP break; case PROP_ERROR_NO_FS: // Command sent without the synthesizer being programmed break; case PROP_ERROR_RXOVF: // RX overflow observed during operation break; default: // Uncaught error event - these could come from the // pool of states defined in rf_mailbox.h while(1); } } } } void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e) { if (e & RF_EventRxEntryDone) { /* Get current unhandled data entry */ currentDataEntry = RFQueue_getDataEntry(); /* Handle the packet data, located at ¤tDataEntry->data: * - Length is the first byte with the current configuration * - Data starts from the second byte */ packetLength = *(uint8_t*)(¤tDataEntry->data); packetDataPointer = (uint8_t*)(¤tDataEntry->data + 1); /* Copy the payload + the status byte to the packet variable */ memcpy(packet, packetDataPointer, (packetLength + 1)); RFQueue_nextEntry(); } }
When I use this code in two launchpad my code work OK, in my first launchpad "action = 1" and in the second "action = 0", I using smartrf_settings.c
#include <ti/devices/DeviceFamily.h> #include DeviceFamily_constructPath(driverlib/rf_mailbox.h) #include DeviceFamily_constructPath(driverlib/rf_common_cmd.h) #include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h) #include <ti/drivers/rf/RF.h> #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h) #include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h) #include "smartrf_settings.h" // TI-RTOS RF Mode Object RF_Mode RF_prop = { .rfMode = RF_MODE_PROPRIETARY_SUB_1, .cpePatchFxn = &rf_patch_cpe_genfsk, .mcePatchFxn = 0, .rfePatchFxn = &rf_patch_rfe_genfsk, }; // Overrides for CMD_PROP_RADIO_DIV_SETUP uint32_t pOverrides[] = { // override_use_patch_prop_genfsk.xml // PHY: Use MCE ROM bank 4, RFE RAM patch MCE_RFE_OVERRIDE(0,4,0,1,0,0), // override_synth_prop_863_930_div5.xml // Synth: Set recommended RTRIM to 7 HW_REG_OVERRIDE(0x4038,0x0037), // Synth: Set Fref to 4 MHz (uint32_t)0x000684A3, // Synth: Configure fine calibration setting HW_REG_OVERRIDE(0x4020,0x7F00), // Synth: Configure fine calibration setting HW_REG_OVERRIDE(0x4064,0x0040), // Synth: Configure fine calibration setting (uint32_t)0xB1070503, // Synth: Configure fine calibration setting (uint32_t)0x05330523, // Synth: Set loop bandwidth after lock to 20 kHz (uint32_t)0x0A480583, // Synth: Set loop bandwidth after lock to 20 kHz (uint32_t)0x7AB80603, // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference) ADI_REG_OVERRIDE(1,4,0x9F), // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1) ADI_HALFREG_OVERRIDE(1,7,0x4,0x4), // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering (uint32_t)0x02010403, // Synth: Configure extra PLL filtering (uint32_t)0x00108463, // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us) (uint32_t)0x04B00243, // override_phy_rx_aaf_bw_0xd.xml // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD) ADI_HALFREG_OVERRIDE(0,61,0xF,0xD), // override_phy_gfsk_rx.xml // Rx: Set LNA bias current trim offset to 3 (uint32_t)0x00038883, // Rx: Freeze RSSI on sync found event HW_REG_OVERRIDE(0x6084,0x35F1), // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A. HW_REG_OVERRIDE(0x6088,0x411A), // Tx: Configure PA ramping setting HW_REG_OVERRIDE(0x608C,0x8213), // override_phy_rx_rssi_offset_5db.xml // Rx: Set RSSI offset to adjust reported RSSI by +5 dB (default: 0), trimmed for external bias and differential configuration (uint32_t)0x00FB88A3, #if (CCFG_FORCE_VDDR_HH) // TX power override // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8) ADI_REG_OVERRIDE(0,12,0xF8), #endif (uint32_t)0xFFFFFFFF, }; // CMD_PROP_RADIO_DIV_SETUP rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup = { .commandNo = 0x3807, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .modulation.modType = 0x1, .modulation.deviation = 0x64, .symbolRate.preScale = 0xF, .symbolRate.rateWord = 0x8000, .symbolRate.decimMode = 0x0, .rxBw = 0x24, .preamConf.nPreamBytes = 0x4, .preamConf.preamMode = 0x0, .formatConf.nSwBits = 0x20, .formatConf.bBitReversal = 0x0, .formatConf.bMsbFirst = 0x1, .formatConf.fecMode = 0x0, .formatConf.whitenMode = 0x0, .config.frontEndMode = 0x0, .config.biasMode = 0x1, .config.analogCfgMode = 0x0, .config.bNoFsPowerUp = 0x0, .txPower = 0xA73F, .pRegOverride = pOverrides, .centerFreq = 0x0364, .intFreq = 0x8000, .loDivider = 0x05, }; // CMD_FS rfc_CMD_FS_t RF_cmdFs = { .commandNo = 0x0803, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .frequency = 0x0364, .fractFreq = 0x0000, .synthConf.bTxMode = 0x0, .synthConf.refFreq = 0x0, .__dummy0 = 0x00, .__dummy1 = 0x00, .__dummy2 = 0x00, .__dummy3 = 0x0000, }; // CMD_PROP_TX rfc_CMD_PROP_TX_t RF_cmdPropTx = { .commandNo = 0x3801, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bUseCrc = 0x1, .pktConf.bVarLen = 0x1, .pktLen = 0x1E, // SET APPLICATION PAYLOAD LENGTH .syncWord = 0x930B51DE, .pPkt = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx }; // CMD_PROP_RX rfc_CMD_PROP_RX_t RF_cmdPropRx = { .commandNo = 0x3802, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bRepeatOk = 0x0, .pktConf.bRepeatNok = 0x0, .pktConf.bUseCrc = 0x1, .pktConf.bVarLen = 0x1, .pktConf.bChkAddress = 0x0, .pktConf.endType = 0x0, .pktConf.filterOp = 0x0, .rxConf.bAutoFlushIgnored = 0x0, .rxConf.bAutoFlushCrcErr = 0x0, .rxConf.bIncludeHdr = 0x1, .rxConf.bIncludeCrc = 0x0, .rxConf.bAppendRssi = 0x0, .rxConf.bAppendTimestamp = 0x0, .rxConf.bAppendStatus = 0x1, .syncWord = 0x930B51DE, .maxPktLen = 0xFF, // MAKE SURE DATA ENTRY IS LARGE ENOUGH .address0 = 0xAA, .address1 = 0xBB, .endTrigger.triggerType = 0x1, .endTrigger.bEnaCmd = 0x0, .endTrigger.triggerNo = 0x0, .endTrigger.pastTrig = 0x0, .endTime = 0x00000000, .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx .pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx }; // CMD_TX_TEST rfc_CMD_TX_TEST_t RF_cmdTxTest = { .commandNo = 0x0808, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .config.bUseCw = 0x0, .config.bFsOff = 0x1, .config.whitenMode = 0x2, .__dummy0 = 0x00, .txWord = 0xABCD, .__dummy1 = 0x00, .endTrigger.triggerType = 0x1, .endTrigger.bEnaCmd = 0x0, .endTrigger.triggerNo = 0x0, .endTrigger.pastTrig = 0x0, .syncWord = 0x930B51DE, .endTime = 0x00000000, };
But when I use the same code in two custome boards for 433MHz, the code don´t work, the first TX (board A) and RX (board B) is OK but when the RX (Board B) try to TX I get these code in debugger
For 433MHz I use smartrf_sttings.c generated by SmartRF Studio
#include <ti/devices/DeviceFamily.h> #include DeviceFamily_constructPath(driverlib/rf_mailbox.h) #include DeviceFamily_constructPath(driverlib/rf_common_cmd.h) #include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h) #include <ti/drivers/rf/RF.h> #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h) #include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h) #include "smartrf_settings.h" // TI-RTOS RF Mode Object RF_Mode RF_prop = { .rfMode = RF_MODE_PROPRIETARY_SUB_1, .cpePatchFxn = &rf_patch_cpe_genfsk, .mcePatchFxn = 0, .rfePatchFxn = &rf_patch_rfe_genfsk, }; // Overrides for CMD_PROP_RADIO_DIV_SETUP uint32_t pOverrides[] = { // override_use_patch_prop_genfsk.xml // PHY: Use MCE ROM bank 4, RFE RAM patch MCE_RFE_OVERRIDE(0,4,0,1,0,0), // override_synth_prop_430_510_div10.xml // Synth: Set recommended RTRIM to 7 HW_REG_OVERRIDE(0x4038,0x0037), // Synth: Set Fref to 4 MHz (uint32_t)0x000684A3, // Synth: Configure fine calibration setting HW_REG_OVERRIDE(0x4020,0x7F00), // Synth: Configure fine calibration setting HW_REG_OVERRIDE(0x4064,0x0040), // Synth: Configure fine calibration setting (uint32_t)0xB1070503, // Synth: Configure fine calibration setting (uint32_t)0x05330523, // Synth: Set loop bandwidth after lock to 20 kHz (uint32_t)0x0A480583, // Synth: Set loop bandwidth after lock to 20 kHz (uint32_t)0x7AB80603, // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference) ADI_REG_OVERRIDE(1,4,0x9F), // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1) ADI_HALFREG_OVERRIDE(1,7,0x4,0x4), // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering (uint32_t)0x02010403, // Synth: Configure extra PLL filtering (uint32_t)0x00108463, // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us) (uint32_t)0x04B00243, // override_synth_disable_bias_div10.xml // Synth: Set divider bias to disabled HW32_ARRAY_OVERRIDE(0x405C,1), // Synth: Set divider bias to disabled (specific for loDivider=10) (uint32_t)0x18000280, // override_phy_rx_aaf_bw_0xd.xml // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD) ADI_HALFREG_OVERRIDE(0,61,0xF,0xD), // override_phy_gfsk_rx.xml // Rx: Set LNA bias current trim offset to 3 (uint32_t)0x00038883, // Rx: Freeze RSSI on sync found event HW_REG_OVERRIDE(0x6084,0x35F1), // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A. HW_REG_OVERRIDE(0x6088,0x411A), // Tx: Configure PA ramping setting HW_REG_OVERRIDE(0x608C,0x8213), // override_phy_rx_rssi_offset_neg2db.xml // Rx: Set RSSI offset to adjust reported RSSI by -2 dB (default: 0), trimmed for external bias and differential configuration (uint32_t)0x000288A3, // TX power override // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8) ADI_REG_OVERRIDE(0,12,0xF8), (uint32_t)0xFFFFFFFF }; // CMD_PROP_RADIO_DIV_SETUP // Proprietary Mode Radio Setup Command for All Frequency Bands rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup = { .commandNo = 0x3807, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .modulation.modType = 0x1, .modulation.deviation = 0x64, .symbolRate.preScale = 0xF, .symbolRate.rateWord = 0x8000, .symbolRate.decimMode = 0x0, .rxBw = 0x24, .preamConf.nPreamBytes = 0x4, .preamConf.preamMode = 0x0, .formatConf.nSwBits = 0x20, .formatConf.bBitReversal = 0x0, .formatConf.bMsbFirst = 0x1, .formatConf.fecMode = 0x0, .formatConf.whitenMode = 0x0, .config.frontEndMode = 0x0, .config.biasMode = 0x1, .config.analogCfgMode = 0x0, .config.bNoFsPowerUp = 0x0, .txPower = 0x913F, .pRegOverride = pOverrides, .centerFreq = 0x01B1, .intFreq = 0x8000, .loDivider = 0x0A }; // CMD_FS // Frequency Synthesizer Programming Command rfc_CMD_FS_t RF_cmdFs = { .commandNo = 0x0803, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .frequency = 0x01B1, .fractFreq = 0xEB9A, .synthConf.bTxMode = 0x0, .synthConf.refFreq = 0x0, .__dummy0 = 0x00, .__dummy1 = 0x00, .__dummy2 = 0x00, .__dummy3 = 0x0000 }; // CMD_PROP_TX // Proprietary Mode Transmit Command rfc_CMD_PROP_TX_t RF_cmdPropTx = { .commandNo = 0x3801, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bUseCrc = 0x1, .pktConf.bVarLen = 0x1, .pktLen = 0x1E, .syncWord = 0x930B51DE, .pPkt = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx }; // CMD_PROP_RX // Proprietary Mode Receive Command rfc_CMD_PROP_RX_t RF_cmdPropRx = { .commandNo = 0x3802, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bRepeatOk = 0x0, .pktConf.bRepeatNok = 0x0, .pktConf.bUseCrc = 0x1, .pktConf.bVarLen = 0x1, .pktConf.bChkAddress = 0x0, .pktConf.endType = 0x0, .pktConf.filterOp = 0x0, .rxConf.bAutoFlushIgnored = 0x0, .rxConf.bAutoFlushCrcErr = 0x0, .rxConf.bIncludeHdr = 0x1, .rxConf.bIncludeCrc = 0x0, .rxConf.bAppendRssi = 0x0, .rxConf.bAppendTimestamp = 0x0, .rxConf.bAppendStatus = 0x1, .syncWord = 0x930B51DE, .maxPktLen = 0xFF, .address0 = 0xAA, .address1 = 0xBB, .endTrigger.triggerType = 0x1, .endTrigger.bEnaCmd = 0x0, .endTrigger.triggerNo = 0x0, .endTrigger.pastTrig = 0x0, .endTime = 0x00000000, .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx .pOutput = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx };