Other Parts Discussed in Thread: TIDA-010003, TIDA-010024
Hi,
I would like to use a mesh topology for a sensor network. I have successfully tested the TIDA-01547 (Simple 6LoWPAN mesh data collector improves network performance) together with the TIDA-010003 (Simple 6LoWPAN Mesh End-Node Improves Network Performance) reference designs.
That's great, but I have no idea about the power budget required for the mesh topology. In my case each node only needs to transmit in case of alarm, so there shouldn't be any traffic 99% of the time but I don't know if the mesh topology management requires extra transmissions and longer awake periods that increase the consumption drastically. Is it possible to put all nodes into sleep mode and wake up periodically to listen/transmit or does the topology require permanently awake nodes and management transmissions?
I need to know the overall mesh consumption to see if we can achieve 10 years battery life with a 3V 1.5Ah
Thanks!
Javi