This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC1310: Clarification on the capacitor of the XOSC (CC1310 or CC26x0)

Part Number: CC1310
Other Parts Discussed in Thread: CC2650

Tool/software: TI-RTOS

I would like to get clarification about the "cap-array" for the 24MHz external crystal of cc1310 (or cc2650), as seen in the MODE_CONF register. How do you calculate the 8-bit value of the array? I haven't found any documentation on this setting? Does it mean that you can avoid installing the two capacitors around the external crystal (8pF in my case)? Is there any performance impact?