This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: CC1352P eval kit power consumption with ble5 project

Part Number: CC1352P
Other Parts Discussed in Thread: ENERGYTRACE, CC1352R, CC1312R

Hi,

I'm using the CC1352P-2 development kit.

Tried measuring the consumption current while running ble5_simple_peripheral_cc13x2p2lp_app and dmm_wsnnode_remote_display_app_CC1352P_2_LAUNCHXL_tirtos_ccs projects.

In both cases I've disabled the advertise, and also the WSN transmissions.

I'm taking the measurements with a continuous current metwe, with 1mS sample rate.

In both cases the average current is a bit more than 80uA, while the minimum current floor is about 80uA.

In this case I'd expect the current to be around 1uA.

Is there any reason for this high current? Maybe it's the on board FLASH device that should be put into deep sleep?

Is there any other options to add to the project, except the POWER_SAVING ?

Is there anything else that should be done in the project to reduce current?

Thanks, Isak.