This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310

Part Number: CC1310

I'm Planning to use CC1310 and Integrating with one motion sensor which consumes 6uA(Running all the time) and will be set to threshold and if threshold crosses through the sensor Controller it'll wake up the MCU and Send the Data once a day and range has to be in K and go back to sleep state.

So i'm planning to set it 14dBm(25mA) and overall a Day consumption will be around 28-29mA .

So I'm planning to use Coin Battery so as to cost cut.

In my opinion CR2032(225mAh) wont be sufficient enough to come for a Years.

So I'm Planning to use Coin Battery Capacity of 1Ah.

Any thoughts on this or should we go to LiPo Battery itself?