This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 - Porting from SDV v2.10 to v2.40 with TI-RTOS support

Part Number: CC1310

Hi,

I would like to ask a question regarding porting existing applications from v2.10 of CC13xx SL SDK to v2.40. I see from the release notes that the pdm I2S has changed and that the driver has been refectored so that the byproduct lib from v2.10 necessary as dependency is obsolete.

In going further I decided to remove this dependency from the TI-RTOS referenced project by my application, especially since otherwise the build will fail along these lines:

makefile:157: recipe for target 'test_flash.out' failed
/opt/ti/ccsv8/tools/compiler/gcc-arm-none-eabi-7-2017-q4-major/bin/../lib/gcc/arm-none-eabi/7.2.1/../../../../arm-none-eabi/bin/ld: cannot find -l:ti/drivers/pdm/lib/pdm_cc13x0.am3g
collect2: error: ld returned 1 exit status

My question is whether deleting this dependency is "safe" or appropriate action going further so it doesn't bite me back. I should specify that I do not use any I2S device nor plan to interact with that functionality at this point in time (cannot say too much about the future though :))

Best,

Andrei