This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: Receive audio in the proprietary mode

Part Number: CC1310

Tool/software: Code Composer Studio

I am working on a project that is a battery remote CC1310 device.

The requirements are it will receive RF in the proprietary mode

The received data is continuous voice and random control data information

The received data need to converted to I2S from the transmitter data if the format is different.

The data is then load into PCM5100APW Digital to Analog converter as the Decoder

Randomly the remote CC1310 needs to transmit status information back to the base station.