This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1125: cc1125: about AGC configuration

Part Number: CC1125

I have the same problem as this post::

e2e.ti.com/.../2893337

and still have no idea to solve it. have 2 question after read that post:

1.Does the RSSI offset make any difference to the way the CC112x works or does it just affect the value reported as RSSI?
2. Cause I use the Synchronous Serial Mode without the cc1125 to detect sync/preamble,does the AGC help our application, since I just disable the AGC behavior(AGC_CFG1.AGC_SYNC_BEHAVIOUR = 000 (No AGC gain freeze, keep computing /updating RSSI)