Other Parts Discussed in Thread: LMH2191
Hello expert,
I'm designing my custom CC1310 board with one CC1310 working as transmitter and one working as receiver. I would like to subtract quadrature amplitude and phase information. Previously, I was only working on amplitude because the phase variations in the transmitter-to-receiver phase relationship has less affect on amplitude. To also check phase information, I would like to have transmitter and receiver sharing the same crystal to avoid phase variation. But I could not find any reference design which two transceiver share the same crystal.
Is it OK to have two CC1310 sharing the same 24MHz crystal?
If I could do it, should I add load capacitors for the crystal? (In all your launchpad designs, you either direct ground them or put Do Not Mount.)
Thank you so much!