I want to use two GP timers in the edge counting mode to generate I/Q signals. For that I need to route two I/O pins to the inputs of the timers for the edge detection. I also need to route the outputs of the timers to two I/O pins for the generated I/Q signals. Would you please send me the code to set up the such I/O pins to the timer connections? Thanks.
Also, is it possible to route the output of a timer in the PWM mode to the inputs of two timers in the edge counting mode without going through the physical I/O pins?