Hello,
In our new design, we will use an aluminium enclosure. After soldering our "CC1310 module" onto the PCB, The uFL to SMA antenna cable will make a connection between the CC1310 module and the external 868MHz antenna.
But the SMA side of the antenna will be touching the conductive aluminium case and uFL side is connected to GND inside the module. So, PE and GND (0V) will be short circuit. Aluminium enclosure will be short circuit to electrical cabinets PE connection.
Can I make a successful wireless communication while GND and PE is short circuit?
Best regards,
Onur