Bought on Aliexspress module:
СС1310 868MHz Wireless rf Module CDSENET E70-868T14S2 iot 25mW Transceiver SMD UART rf Transmitter Receiver 868 MHz SOC Module
When trying to write a program to CC1310F128 RSM (4x4mm package) installed in this module, an error appears through the program Code Composer Studio:
Error connecting to the target (Error -241 @ 0x0)
A router subpath could not be accessed. A security error has probably occurred. Make sure your device is unlocked. (Emulation package 8.0.27.9)
When recording the same program in CC1310F128RGZ installed in another module, there are no errors, everything goes well.
Help, if anyone faced such a problem.
Vladimir.