Other Parts Discussed in Thread: AES-128
Tool/software: TI-RTOS
Hi
I try to make a simple network application to use Easylink.
But, I don't know what differences between Easlink and TI 15.4 Stack are.
I'd like to compare with TI 15.4 stack and Easylink.
Maybe, some of the functions are not supporting such as security.
Could you let me know the difference refer to table as below ?
I try to use rfWsnConcentrator and rfWsnNode example when I can make a sensor network to use Easylink.
1. Do rfWsnConcentrator and rfWsnNode have security feature? If not, what example can I follow to implement security feature?
2. Do rfWsnConcentrator and rfWsnNode have device association and disassociation feature? It is because I cannot find any easylink API related to device association and disassociation.
3. Could Clear Channel Assessment (CCA) Cofiguration replace CSMA/CD or LBT function ?
802.15.4 Spec |
TI 15.4 Stack |
Easylink |
|
Devices specified |
Network Coordinator Full function Device Reduced Function Device |
Coordinator Sensor |
Coordinator Sensor (Node) |
Frame structure |
Data Frame Acknowledgment Frame MAC Command Frame Beacon Frame Optional superframe structure Traffic types MAC data service /Primitives Optional GTS mechanism (guaranteed time slots) |
Synchronous (beacon) and asynchronous (non-beacon) |
?? |
Association/ disassociation |
Access to the PIB Association /disassociation GTS allocation Message pending Node notification Network scanning/start Network synchronization/search |
Network and device management – joining, commissioning, service discovery |
?? |
channel Access |
CSMA-CA channel Access |
Medium access with CSMA/CA and LBT |
Clear Channel Assessment (CCA) |
Security |
AES-128 |
Pre-shared key AES security |
Not supporting |