This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: Packet error and CRC Error in CC1310 LaunchPad

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

Hy ,

We tested the range of CC1310 using 2 CC1310F128 LaunchPad in an Open space.(150-200m).

First we tested in this setting:

5Kbps SimpleLink Long Range (20 kchip/s , 2GSK,conv.FEC r=1/2 K=7 DSSS SF=2, Tx dev: 5KHz,Rx BW=49KHz).

It was all fine able to receive the packet from 200m (PCB Antenna).

But 625 bps Legacy Long Range (10 kchip/s , 2FSK,conv.FEC r=1/2 K=7 DSSS SF=8, Tx dev: 5KHz,Rx BW=40KHz).

Same PCB Antenna:

625 bps Legacy Range 38 sent

31 Received Ok

Packet Errr 6.1%

Bit Errr rate 0.03%

19:25:14.903 | 96 | 46025 | e9 fe 85 2a 2d 02 8e 08 32 7d b1 6b 73 a1 a2 9b 0a 96 0f 9a 59 19 aa af ee fd 61 d4 b6 c7 59 9e 1a 7e 8b 45 2a 51 ce 96 30 79 48 3f 6e 0d ad 78 ba ff 5c 5c 51 2b 71 f5 14 fc 8c 2b f8 a7 73 5d aa 00 a2 bb 4f e9 ed 9a 1c 84 52 72 da 9e 77 c7 e1 7b 47 cb 7d 9c ef 0d 5a a3 c6 6a e3 37 d5 df e3 12 18 4e 30 93 3b 74 f7 48 2a b2 0c bf 0e ff 33 38 42 b0 95 76 27 6b b9 f1 82 16 0a cd 1d 40 15 c6 df be be a9 9a d3 f6 03 6b 39 7b 3e 52 25 b4 46 6a 1d | -100 CRC error

19:25:17.202 | 14 | 0000 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -97 CRC error

19:25:21.184 | 14 | 0007 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -88

19:25:21.762 | 14 | 0008 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -95

19:25:22.331 | 14 | 0009 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -97

19:25:22.894 | 14 | 0010 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -91

19:25:23.473 | 14 | 0011 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -82

19:25:24.047 | 14 | 0012 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:24.632 | 14 | 0013 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -80

19:25:25.202 | 14 | 0014 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:25.761 | 14 | 0015 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:26.329 | 14 | 0016 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -80

19:25:26.907 | 14 | 0017 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:27.477 | 14 | 0018 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -83

19:25:28.047 | 14 | 0019 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -84

19:25:28.629 | 14 | 0020 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -83

19:25:29.191 | 14 | 0021 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -86

19:25:29.769 | 14 | 0022 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -83

19:25:30.333 | 14 | 0023 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -86

19:25:30.915 | 14 | 0024 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:31.481 | 14 | 0025 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:32.047 | 14 | 0026 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -84

19:25:32.625 | 14 | 0027 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:33.191 | 14 | 0028 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -79

19:25:33.769 | 14 | 0029 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -78

19:25:34.335 | 14 | 0030 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -78

19:25:34.918 | 14 | 0031 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -78

19:25:35.486 | 14 | 0032 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -79

19:25:36.048 | 14 | 0033 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -78

19:25:36.629 | 14 | 0034 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -79

19:25:37.202 | 14 | 0035 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -78

19:25:37.772 | 14 | 0036 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

19:25:38.342 | 14 | 0037 | 02 42 17 4c 42 91 40 cd 08 9c 43 99 64 88 bf a4 0a 89 | -81

What can be cause for the CRC Error?

What ways to decode those?

Some times when the RSSI was -92 there was CRC error and sometimes even in -83 there was CRC error.

Next day when we tried with the same setting 5Kbps but not in Open space, 

There was a 23%-32% of packet Error.

We are yet to test with the External Antenna.

There's UFL Connector in CC1310 LaunchPad Any suggestion for the External Antenna(Flat Patch/ other) ?