This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: SmartRF Flash Programmer 2 command line -rs reset is not working

Part Number: CC1310


I'm using command line to program the board cc1310 launchpad. The programming erase and reset works fine if I do 

srfprog -t soc(XDS-L2000XXX,CC1310) -e -p -v -f p:\CC1310_CC1310DK_7XD_TI.hex 

Start flash erase ...

OK

Reset target ...

OK

but if I want to just reset the board then it throws error. I went through documents but it doesn't seem to be clear to me. Used below command to reset

srfprog -t soc(XDS-L2000J89,CC1310) -rs pin

it does't work

This is the error

The Environment variable "SRFPROG2" seems to be missing!

Texas Instruments SmartRF Flash Programmer 2 v1.8.0-windows
-------------------------------------------------------------------------------

ERROR: Unknown Action: 0

I tried to get examples but didn't help

C:\Program Files (x86)\Texas Instruments\SmartRF Tools\Flash Programmer 2\bin>srfprog -rs ex

The Environment variable "SRFPROG2" seems to be missing!

Texas Instruments SmartRF Flash Programmer 2 v1.8.0-windows
-------------------------------------------------------------------------------

ERROR: This reset option does not exist.
See help documentation for a detailed description of the reset options.

Any input would be helpful