This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Does CC1352P support frequency band of 330~350MHz?

Part Number: CC1352P

I'd like to know if CC1352P support frequency band of 330~350MHz?

I want both 20dBm Tx power and 330~350MHz frequency band. Is there any other choice?

  • Hi,

    There are no characterised RF settings available for that frequency band as of now. Can you elaborate more about the application this is for?

    Regards,
    Fredrik
  • Hi, Fredrik

    Our requirement is mesh (e.g. 6LoPWAN) with middle data rate(e.g. 50kbps of 802.15.4g) at frequency band of 330-350.

    "There are no characterised RF settings available for that frequency band as of now". Do you mean there's no such settings for cc1532p or for all the sub-1G chips?

    For mesh with 50kbps, 20dBm Tx power, 330-350MHz band, is there any choice?

  • Hi,

    You are correct, there are no settings for the 300 MHz frequency band. I would recommend you to consider either 868/915 MHz or 433 MHz instead. The latter is not currently available either, but will be added later this year.

    Regards,
    Fredrik