This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-15.4-STACK-GATEWAY-LINUX-SDK: Doing this project with the BBB wireless instead of a regular BBB and a cape

Part Number: TI-15.4-STACK-GATEWAY-LINUX-SDK


Hello all,

I am following this guide for this project:  

dev.ti.com/.../154-stack_03_linux_project_0.html                  

But instead of using the BBB and a wireless cape , I am using the Wireless BeagleBone Black.

I am not sure which of the steps in step 4 I should ignore in this case , since the BeagleBone Black wireless does not have an ethernet port. It seemed to me first that number 10 in Step4a is where I need to go after finishing task 3, but then that would mean that I won't use the image am335x-evm-linux-03.02.00.05.img.zip it asked to download in step 1 in 4a?

I would like as much explanation as possible on this please. Which are the steps from 4a and 4b that I need to do If I were to use the BBB wireless instead of a BBB and a wireless cape.

Thank you.

Best regards.

Neil.